Other Parts Discussed in Thread: BQ25713
Tool/software:
Hi,
I would like to turn off the power path by setting FORCE_LATCHOFF = 1. The flag is set correctly when I read back the register, but I still measure a regulated output voltage VSYS = 14.15V and CHRG_OK does also not go low. I would expect to measure battery voltage VBAT = 13.75V. The BQ25713 is in default configureation (POR) with connected input voltage of 12V nad a battery voltage of 13.76V.