This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650864: PMIC o/ps are not stable

Part Number: TPS650864


Tool/software:

Hi

We are using PMIC TPS6508641 to power Zynq ultrascale+ XQZU19EG-2FFQB1517I.

We are using 6V to power the PMIC. The PMIC o/ps are not stable. The below is the capture at buck1 output 5V. and its feedback signal FBVOUT1.

5V output:

FBVOUT1:

Buck2 o/p:

We removed R32(please refer schematics below) and checked. Then pmic output 5V is ok but still feedback is not ok

Below is our schematic:

Please note we are providing 6V to both PMIC Vsys and U5 drain. Also we provided external LC components to LX5 and have disconnected FB5 from gnd and connected to a o/p cap.