Tool/software:
Hello,
As I read the datasheet, it appears to me that the chip will enter standby mode when the voltage at EN/UVLO pin falls below 1.4V +0.04V/-0.05V (referencing V_EN-FALLING in the Electrical Characteristics table in section 5.5). By the same logic, I have reason to believe the part will exit standby mode and enable when the voltage at the EN/UVLO pin raises above 1.5V +/- 0.05V (referencing V_EN-RISING). I anticipate my understanding is wrong, as it would suggest there is a possibility the part could enter standby mode as the EN/UVLO voltage lowers to 1.44V and could enable again quickly if there was enough noise on the signal to raise the voltage back up to 1.45V.
Please clarify how these EN/ULVO rising and falling parameters should be interpreted. As I understand it now, there is not enough hysteresis on the EN (standby) thresholds.
Thank you.