Tool/software:
Hi Garrett,
Another follow up question to the foggy issue we sometimes have here....however this time we discovered a definite issue and I'm wondering if/how it impacts the BQ24070.
In our system there is a power switch effectively connected to the OUT pins that connects power to the board when it is closed. When the switch is closed, the OUT pins will see the 222uF that are the input caps on a (TI) boost converter.
Assume the switch is open.
The BQ24070 is connected to an 18650 battery (no switch) and the OUT pins are connected to the switch.
When the switch is closed, there is a large inrush current to charge up the 222uF caps.
This inrush current exceeds 4A. (Probably tries to be 2-3X that)
2 Questions:
[1] Will this high current draw cause a protection circuit to kick in resulting in only a 2V output from the chip until it is power cycled.
[2] Could this inrush current damage the part and result in the failure mode we've seen 3 times now. That is, the device charges the battery, but never recognizes the fully charged state. (as least by the status indicators).
I asked and you responded to a very similar question on Nov 13, 2024, but I thought I'd send the message above to make sure I'm not missing anything.
Thanks and Best Regards
Jerry Molnar