Other Parts Discussed in Thread: LMR36520,
Tool/software:
Dear Experts,
Greetings from Istanbul.
I am currently having a problem to my Non-Isolated Buck (Fly-Buck) both inverting and non-inverting Converter
My aim is to generate a positive 1 Amper +6V and 0,5A negative -5,7 V voltage. ( values are not sensitive )
However, when I power up voltage between 12V and 24V to the circuit, although there is no load, the LMR33640DDDAR immediately getting too hot. Can not touch by hand in 1 sec.
At the same time, when I measure, I see -5V on the negative side and 2.5V output on the positive side.
My Material List in the diagram is as follows;
- I'm using the LMR33640DDDAR at 1 Mhz one.
- Coupled inductor is SRF0703-4R7MCT.
- Other components are listed in the scheme,
Could you please have a look where i m stuck ?
Best Regards