This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25730: Charge Behavior for 1S battery, 5V input charger.

Part Number: BQ25730


Tool/software:

Hello, using the EVM and wondering what the behavior should be for charging 1S battery in range of 3.2 - 4.2V.
1S config is set on JP3
OTG jumper block JP2 is attached.

If I write to charge current register (0x02) the data 0x40 0x00 this should set the charger to deliver 128mA
If I set charge current to 0x00 0x02 I would expect 1A current.

I've used a DMM setup to measure the current into the battery and can confirm it sinks current.
It is a 2200mAh 3.7V single cell lipo.

The results I obtain are not what I expect however as writing 0x40 0x00 delivers ~ 150mA
0x00 0x02 delivers ~ 250mA.