Tool/software:
I am going to use UCC256601 to design an adjustable power supply whose output voltage is from 0 V to 300V with input voltage 170VAC -240Vac . Could the UCC256601 be used ?
thanks,
John
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am going to use UCC256601 to design an adjustable power supply whose output voltage is from 0 V to 300V with input voltage 170VAC -240Vac . Could the UCC256601 be used ?
thanks,
John
HI John,
You can not use LLC for such a high output voltage range. Please create a different thread without using the controller's name. You would get a topology suggestion for this application.
Regards
Manikanta P
Hi Manikanta P,
Can the LLC use for the input voltage range for 170VAC-240VAC ,right ? The LLC provide what the output voltage range is ?
HI JOhn,
You can use LLC for 170-240V AC.
LLC's are more efficient when max gain from input to output requirement doesn't exceed 2.5- 3.
Regards
Manikanta P