This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR38020QEVM: Operating temperature

Part Number: LMR38020QEVM


Tool/software:

Hi,

I would like to evaluate the LMR38020QEVM under high temperature and low temperature.
What is the operating temperature range of this evaluation board?

BR,

Taku

  • Hi Taku,

    The EVM can be used at the same temperature range as the device i.e. operating junction temperature (TJ ) range of –40°C to +150°C. Please note that the ambient temperature range would be less than this as the  Junction temperature = Ambient temperature + P_D∙θ_JA.

    P_D = Power loss in converter (W)

    θ_JA = Thermal resistance from junction to ambient (°C/W)

    Regards,

    Niranjan