Other Parts Discussed in Thread: LM61440
Tool/software:
Hello,
My customer is looking for a power supply with the following requirements:
- Input Voltage: 28V or 36V
- Output Voltage: 4V to 27V
- Output Current: 50mA to 4A
- Application: Motor power supply
- Preferences: Integrated solutions where available
- Control Method: Voltage controlled via microcontroller, likely using a DAC
Do we have any options with a flexible output voltage that can be controlled by an MCU DAC?