This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLVM23625: temperature images and efficiency of TLVM23625

Part Number: TLVM23625

Tool/software:

Hi,

The datasheet shows thermal camera images indicating that the TLVM23625 heats up more at lower operating frequencies. This doesn't match the fact that efficiency worsens as the frequency increases.

What's the reason for these images? Or maybe I'm misinterpreting something...

Vin=12V Vout=3.3 2A @ 1MHz = 57.9 ºC

Vin=12V Vout=3.3 2A @ 2.2MHz = 53.1 ºC

BR