Other Parts Discussed in Thread: PMP31092, UCC2808A-2, LM25037
Tool/software:
Need a fast resolution: can we do a step up converter using ACTIVE CLAMP FORWARD controllers?
Input: 22 to 32VC DC
or can have it boosted to 200V using another TI REF Design module such as AC Flyback- which has isolation.
Wont really want to have 2 isolation transformers.!
Output: 100v
power : 300 W
Since there is a transformer, is there anything topologically impossible with 1:N step up conversion? Apart from the PMOS, will be using all GaN devices.
I tried to use "Power Stage" designer, it just would not take these inputs and outputs!
Will appreciate a fast resolution of this..-
r