Other Parts Discussed in Thread: BQ40Z50-R2, BQ28Z620
Tool/software:
I have a need for a one-wire communication battery manager for a 2S pack that ALSO will wake up under a certain condition.
The BQ78Z100 can be setup to switch off after 1 minute of no communication.
But there is no way to wake it back up based on the communication line, instead a positive voltage must be applied to the Pack+
Are there ANY one wire interface chips that would, for example, leave the HDQ line weakly pulled up when the pack is off, so that pulling down the line would wake the pack back up?
It would be like having the /PRES line of an SMBus battery pack being shared with the HDQ line.
Other suggestions for making a one-wire communication battery pack that can be woke up and put to sleep using only that one wire would be appreciated.
We have at least a dozen battery systems already using TI chips, so our preference is to stay with TI.