Other Parts Discussed in Thread: BQ25071
Tool/software:
We have download a new Golden Image from the CPU, will bq27z746 use the new settings without any command or do do we need to send a reset command?
We have big problem with the reset command when we short circuit the FETs (R202 = 0 ohm was mounted). The reason for shot circuit the FETs was to high current from motors that trigger the bq27z746 short circuit mode. It seems like the bq27z746 got in a "latch-up" mode and the chip got very hot. The only way to get it to work again was to let it discharge the battery to <1.8V. Then it worked as normal again.