Other Parts Discussed in Thread: BQ25798, , TPS25750, TPS25751, TUSB8041, CSD87501L, TPS54531
Tool/software:
I am design PD system based off the USB-PD-CHG-EVM-01. I have upgraded my TPS25750 to TPS25751 per another thread with Chris. I have questions on the BQ25798 and wonder if I could get a bit of clarification:
Base System - 4 Cell Li-Ion batteries, The USB-C will provide power (sink mode) as well as connected to TUSB8041 hub. The system will also have a barrel connector to power & charge the batteries.
1 - The BQ will have 2 input, Barrel Plug (20V DC), and USB-C to charge and power the system. I am using the CSD87501L and wondering if I have them wired correctly. (see attached schematic)
2 - I am seeing leakage on the USB-PD-CHG-EVM board with nothing connected but the battery pack. What could we redesign to reduce the leakage. I know TPS54531 & TLV7553 will draw power for the TPS25751. Are they needed to be on? Can I tied the EN to the SPST Power control? I did look at "Ship FET mode" on the BQ, but it needs to be set via I2C. I don't think it will be an option since power on would require a barrel connection. I would like to reduce leakage as much as possible, but still be able to charge the batteries with the system is off via barrel or USB-C.