This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH-CIRCUIT-DESIGNER: LMQ644A2QRXARQ1

Part Number: WEBENCH-CIRCUIT-DESIGNER

Tool/software:

In Webench, I am in the process of plugging in a select power inductor for a Buck switching design. The part is not listed so, I created one close to the parameter limitations. This is a interleaving design so there are 6 inductors. 

So next the selected inductor gets the updated parameters with the. Custom created inductor. Next I select the. Next inductor and try to find the part that I just created. And it will not list for me to select it. This seems like a Webench Bug. Another question is where does it put these Custom inductor parts. Is it stored anywhere locally?

Note: The inductor that I created has a higher resistance than was automatically put in the inductor parameter limitations prior to creating the custom part. I wanted to run with it anyway because it is something that is in the supplier catalog and I wanted to check performance with that part.