Tool/software:
Dear Authorised,
We are using the BQ76952 Module with our MCU but we have some problems. We designed a board and we can't communicate between MCU and BQ76952, also when we read the voltage in BREG Voltage we read 0.7V but we guess it should be 5.5V. We also have EVM module, when I try the communication between MCU external I2C and EVM external I2C, it works fine. How do we verify if our BQ76952 could be fitting?