Tool/software:
Hi,
we are trying to determine the overall accuracy of our current measurement . which uses the IMON from TPS4812-Q1
there is a table which provides the Accuracy for particular Vsns input
and there is also this equation:
question :
1. which should be considered ? the two dont match .
2. the formula changes only based on Vsns is this correct if Voffset is constant?
3. Please provide plots Voffset vs temperature and input supply