This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22995H-Q1: VIN=VBIAS <0.8V, VON=3.3V condition, what VOUT status it has?

Part Number: TPS22995H-Q1


Tool/software:

Hi Team,

For TPS22995H-Q1 operating condition.

VIN=VBIAS <0.8V, VON=3.3V condition, what VOUT status it has?

BR.

Lenny Lee.

  • Hello Lenny,

    I need to check this condition on EVM and update you.

    There should be internal VINPOR which enables after 0.8V but need to confirm this hypothesis testing on EVM.

    I will update by tomorrow EoD.

    Thanks 

    Amrit

  • Hello Lenny,

    Sorry for the delay.

    Min bias voltage for this device is 1.5V.

    VIN=VBIAS <0.8V, VON=3.3V condition, what VOUT status it has?

    With this you will VOUT same as VIN with no load. With VBIAS less than the recommended value, RDSon value will be high, and it will not match with the datasheet value.

    You can keep VBIAS more than 1.5V and VIN :0.8V for better RDSon.

    Thanks 

    Amrit