This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74502H: Used for driving back-back power mosfets?

Part Number: LM74502H
Other Parts Discussed in Thread: TPS4800-Q1, TPS1200-Q1

Tool/software:

The datasheet states that the gate driver is capable of driving 11mA but sinking 2,3A. This driving current does not sound as much. I ned a gate driver to drive 2 x 4 N-Channel mosfets (back-back) which act as charge/discharge path switch in a big battery pack. I do not need ultra fast switching but I need a static driver. Each fet has an Ciss of 6nF.