Tool/software:
Hello,
I have produced a completely identical circuit using the BQ76915EVM schematic file as a reference. I am currently trying to connect to BQ76952 via I2C. However, communication is not established.
I also have an EVM module. I can provide I2C communication with this module. When we make the same connection in our own circuit, the connection is not established.
I see 1.804V voltage on the REG18 pin.
The BREG pin shows a voltage that does not change very often around 4-5V.
I feed the BAT pin with 14.46V (I test with 4 series Li-ion batteries).
I see 25.18V on the CP pin.
When I compare these values with the EVM module, everything seems fine