This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61500: Output Capacitor Selection for TPS61500 Backlight Driver Circuit

Part Number: TPS61500

Tool/software:

Hello Support Team,

I am designing a backlight driver circuit using the TPS61500 and have selected a switching frequency of 1.2 MHz to minimize the power stage components and reduce the physical size of the design. Below are the details of my circuit:

  • Input voltage: 3.3V (range: 3.0V to 3.6V)

  • Output voltage: 25V (24.8V + 0.2V FB voltage)

  • Maximum output current: 200mA

  • Switching frequency: 1.2 MHz (range: 1 MHz to 1.4 MHz)

  • Maximum ambient temperature: 70-75°C

I have two capacitor options and would like to know which one is more suitable for my design.

  1. Option 1: 2 x 4.7 µF, 50V, 0805 capacitors

    The self-resonant frequency of this option is around 3 MHz, but with DC bias up to 80%, the effective capacitance at 25V will be reduced to 1.88 µF.

  2. Option 2: 2 x 4.7 µF, 50V, 1206 or 1210 capacitors

    This option provides an effective capacitance of 5.17 µF at 25V, but the self-resonant frequency is around 1.8 to 2 MHz.

Given that the recommended operating conditions suggest a minimum output capacitance of 4.7 µF, and the notes on page 15 recommend a capacitance range of 1 µF to 10 µF.

Which option would you recommend for my circuit?

Best regards,

Malek