This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H6003-SP: TPS7H6003-SP 5V input

Part Number: TPS7H6003-SP
Other Parts Discussed in Thread: TPS7H5001-SP, , TPS7H5020-SP

Tool/software:

Hello

I have a system that is doing a 5V to 0.8V using the TPS7H5001-SP and TP7H6003-SP as a buck controller.

What I missed, is that the TPS7H6003-SP won't take a 5V input. Is it still possible to use the TPS7H6003-SP with a 5V Input? And if it can't work with a 5V Input, is there an example of a boost circuit to go from 5V to 14V?

Thank you

Albert