Other Parts Discussed in Thread: LMR33620, LMR36006, TPS61022, LM43603
Tool/software:
Hi, We are using LMR66420 for a design with the following requirements:
- Vin = 24VDC,nom (19-29VDC)
- Vout = 5VDC
- Iout = ~70mA,nom (100mA,max)
We do not have stringent requirements on Vout ripple or transient respond speed.
My understanding from various TI documentation is that it will operate in PFM 100% of the time at the above loads.
The datasheet has limited information regarding the calculations required to select suitable components (Cin,Cout,L) when the part is in PFM.
I have tried using WEBENCH, but it is very limited in what information is available for this part as it does not enable the simulation part of WEBENCH.
I have been using the following to attempt to understand the expected operation of this device, could you please advise the suitability of these resources for the LMR66420 and if they are not applicable, please provide alternatives:
- SNVC234 - Mode Transitions Calculator LMR336x0 LMR360xx
- SNVA857 - Understanding Mode Transitions for LMR33620/30 and LMR36006/15
- SSZTAL7 - Input and Output Capacitor Considerations in a Synchronous Buck Converter
- SLVAFC3 - Mechanism of TPS61022 PFM and Load Threshold between PFM and PWM for TPS61xxx Converters
- LM43603 Datasheet - Utilizing the component selection calculations
I am particularly interested in the following:
- Component selection based on the design inputs when in PFM
- Calculating the mode transition point out of PFM, based on component selection.
- Vout ripple when in PFM
If there is a SPICE model for this converter, that would be ideal.
We are not considering using any alternative parts at this stage, unless the LMR66420 is expected to be unreliable in this configuration.