This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3762-Q1: TPS3762-Q1 Pspice model

Part Number: TPS3762-Q1

Tool/software:

TPS3762-Q1 Pspice model is not available in Pspice for TI tool. Could you please share the design for the same. 


Below are the following specifications:

Input voltage range: -36V to -60V (Till -80V can be considered) (for telecommunication negative input will be used and positive is taken as return path)

Input Current: 1.5A

Application: UVLO < -36V and OVLO > -60V (Gateway for Telecommunication)

For design support could you please share the contact person details.

Thanks, and regards!