Other Parts Discussed in Thread: BQ25792
Tool/software:
Dear Sirs and Madams,
We have configured the BQ25792 and TPS25751 as a DRP(power sink / source) as shown below, without using external EEPROM.
So I have a question.
I understand that if the battery is valid, there is no problem with DRP negotiation.
If the USB Type-C AC adapter is connected to the USB Type-C connector when the battery is at its lower operating limit voltage and cannot be used, will negotiation be possible normally?
When the battery voltage falls below the lower operating voltage limit, no voltage will be applied to PPHV, PP5V, and VIN_3V3 of TPS25751.
In that state, the TPS25751 should not start.
Even if a USB Type-C AC adapter is connected, I believe that negotiation will not start because EEPROM cannot be read after POR.
After the USB Type-C AC adapter is connected, will we be using 4CC commands to configure TPS25751 and BQ25792, followed by SSrC commands for negotiation?
Regards,
Masashi