Other Parts Discussed in Thread: TPS53355
Tool/software:
Hi,
I am using LMR36510 for our application.
Vin = 24V, Vout = 12V, Iout = 0.015mA.
I need to margin the output voltage via external DAC. May be +30% to -30%.
Could you please tell me, how can I connect the DAC output in order to change the Vout of the LMR36510?
I am attaching the circuit which I used
And also, please suggest a voltage DAC for margining it
Thanks