This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61094: Do you have any device which has higher output capability than TPS61094?

Part Number: TPS61094

Tool/software:

Hello guys,

One of my customers is looking for 5V power supply back up solution with 5F single supercapacitor for 30 seconds.

Their condition is the below.
VIN 5V, VOUT= 5V, Iout 600~800mA, Super-cap voltage =2.7V, the number of cell =1.

They think TPS61094 is good device for their solution. But the device output current is not enough for their load.

So the following is my question.

Q.
Do you have any device which has higher output capability than TPS61094?

Your reply would be much appreciated.

Best regards,
Kazuya.