Tool/software:
I am building a 6kw boost converter that takes 120Vin and produces 340Vout, however I am having some issues with feedback on the UCC28220 chip. I'm using a 200kHz switching frequency, with 10uH inductors on each phase. For current sensing, I have a ACS758ECB-200U-PFF-T hall-based current sensor.
For some reason, the output voltage varies drastically under load. If the no-load setpoint is 80V, under varying loads, the voltage will sag down to nearly the input voltage. It appears as if the feedback loop is very slow to respond, as when removing the load, the voltage will climb for several seconds before slowly approaching the no-load voltage again.
To rule out any current sense issues, I have tried disconnecting the current sensors from chip, so the CS pins both have 0V. Below is a screenshot of the schematic - I'd be happy to provide both the full schematic and layout if needed. Please note that I have changed the resistors for UVLO and OVLO, and I can confirm that these pins are within the operating range, and soft-start is present.
If you could suggest a way to fix the voltage variation problem, that would be greatly appreciated.