This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51561H-Q1: LM5156HQPWPRQ1

Part Number: LM51561H-Q1


Tool/software:

Hi,

What is the maximum soft start time on conveter?

Can the CSS be as example 22uF or 47uF?

The input voltage is 24V the output is 105V/1A.

Many thanks.

Kind regards.

A. Kangani