This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z758: BQstudio Burning issue

Part Number: BQ27Z758
Other Parts Discussed in Thread: BQSTUDIO, , EV2400

Tool/software:

1. For the sample of BQ27Z758, it was found that using the config file of 27Z746, the upper computer BQSTUDIO can automatically connect and pop up the BQSTUDIO communication interface.

  1. When using the 27Z758 config file, it is necessary to manually select to force the BQSTUDIO interface to open, and the connection cannot be automatically popped up.
  2. Both of the above methods can be used to connect and communicate with the product. However, it has been found that after burning the file recommended by TI, the product will disconnect from communication with BQSTUDIO. No matter what attempts are made later, communication cannot be successfully linked.
  3. The latest version of the upper computer software used is 1.3.127

https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/196/bq27z758_5F00_v0_5F00_01_5F00_build_5F00_1.srec

Could you help to comment on this?