This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63020-Q1: Low efficiencies as buck-boost converter for IoT sensor

Part Number: TPS63020-Q1

Tool/software:

Hi,

I'm using the TPS63020-Q1 as a 3.3V buck boost converter for a lithium-ion battery with an input range of 2.6V to 4.1V. This powers a BLE module which, depending on the transmission level spikes between 30-100mA, but has an average current around 100-450uA, when I externally supply the 3.3V. However, when I apply 3.3V through the regulator, it takes around 6-7mA of current, which is way too high for my application. The output voltage is at least correct. Is there any way to improve the efficiency here? I am using a 2.2uH inductor, which is what the data sheet suggests for lower current draws. Do I have any options?

  • Hi   Ryan,

    It is an automotive application? and automotive-grade is must ? Ask just because we have some better device for low load application, but they are not automotive-grade.

    Also, Can you help to check if your device is set at PFM mode?

    Regards

    Tao