Other Parts Discussed in Thread: LMR43610
Tool/software:
Hello ,
I need a dcdc inverter to provide -6V5 from 6V5. I find the LMR14020. fig 8-2 in the datasheet.
I download the uncrypted model. Inside this model there is R_R1 GND 0 = 1m. Due to this line the simulation doesn't work.
Do you confirm that I can change R_R1 to 1meg and do fig-2 without hidden pb.
(simu is ok w/ r_r1 = 1meg)
Iout = 50 to 100mA. Do you see another product that could better fit?
Best regards,