This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22992: Behaviour under over load conditions

Part Number: TPS22992

Tool/software:

Hello, 

How will the TPS22992S behave in case of over load conditions (not short circuit) ? 

For example, if VIN=4V and the output is loaded with a 0.5Ohm resistor, what will happen? 

 Will it limit the current to 6A? Can it get damaged in this case?

Thank you in advance,

Alex