This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3423: Reset IC recommendation

Guru 12815 points

Part Number: TPS3423
Other Parts Discussed in Thread: TPS3421

Tool/software:

Hello,

My customer is looking for a reset IC which can support the following features:

   

If there is a suitable product among TI products, please recommend it.

Thank you.

JH

  • Hi JH,

    The best solution that we can offer is the TPS3421 which has below implementation.

    This design takes advantage of the TS=VDD, which gives the device a 0s press time. 

    And it's dual push button behavior. This setup will implement the logic table above.

    Also the VDD of the first TPS3421 should be 1.8V and the VDD of the second TPS3421 should be 5V

    TPS3421ECDRYR

    Jesse