This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51388: Webdesigner reports 1MHz frequency despite MODE pin is connected to VCC

Part Number: TPS51388

Tool/software:

Hi, I have created design using WEBENCH  from link under the part page:

https://www.ti.com/product/TPS51388 , specifying Vin 11.5-16V, Vout =3.3V , Iload=3A, T=70CThen In configuration options I have chosen f switch =600kHz, and OOA operation.

It looks like simulation is not enabled for this design , can you state if this is ongoing work and you will enable sim ?

If I go to export page , which lists design paramteres I can see schematic ( same as in Customize page) where MODE pin is connecte dto VCC for 600kHz operation), however parameter Frequency listed below schematics shows 986.4kHz despite it should be 600kHz?  Looking at the data sheet operation with 600kHz is permittable in OOA mode. Is it error in webench or does thios device not allow 600kHz operation in OOA mode?

Kind Regards

Sebastian