Tool/software:
The specific part I am using is the TPS35AA38AGADDFRQ1.
Can the watchdog time scaling feature via the SET0 pin be used with a watchdog timeout that is adjusted with a capacitor on the CWD pin? Or, is the watchdog time scaling for devices with a fixed watchdog timeout only?
I want to adjust the timeout to 8 seconds. The part number above has the option to apply a multiplier of 128.
8s/128 = 62.5ms
CWD Capacitor = 0.0625s / (4.95*10^6) = 12.63nF
Thanks.