Tool/software:
Hi,
I want to use the BQ25820 to charge a LiPo accu with a solar cell and supply the board.
The solar cell provides 5V with 2-4W. The akku is a LiPo 3,7V with 27Ah. The system voltage is 3,7V.
If the solar cell powers the device, Q1 and Q2 are open. To supply the system Q3 has also be open. If both MOSFET are open how will be the system voltage regulated? I read the datasheet, bu I don't understand the theory of operation.
Can you help me.
BR
martin sauer