Tool/software:
Hi team,
I have a question regarding the Regulated output accuracy listed in the datasheet.
1.The voltage accuracy is specified for two types, Tj=25℃ and Tj=-40℃ to 150℃.
Is the temperature characteristic ±0.25%?
Or does this mean that ±0.75% is added to the ±0.5%?
2.It seems that the temperature characteristics differ depending on the package. Can you tell me why?
Best regards.