This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM70840-Q1: LM70840-Q1 - design calculations

Part Number: LM70840-Q1
Other Parts Discussed in Thread: LM70840, LM70880

Tool/software:

I need to design a buck converter with below specifications:

Input voltage: 17V to 63V.

Output voltage: 12V.

Load current: 1.5A max.1.2A Typical.

Ambient temperature max.: 85 deg C.

Output capacitor: Electrolytic + Ceramic.

Inductor: Shielded.

Please provide the peripheral component values with calculations.