This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H000-Q1: GND network: Which ground connection of input pins?

Part Number: TPS1H000-Q1


Tool/software:

Hello,

I intend to use a GND network according datasheet to implement reverse-current protection (see Fig. 30)

I use the following values: Resistor 1k, Diode Nexperia BAT46WJ

Datasheet requires diode Vf<0.6V. Vf of BAT46WJ: max. 0.35V @ 10mA / max. 0.475V @ 50mA.

To my question: regarding connection of CL pin, there is following note: Note that if using a GND network which causes a level shift between the device GND and board GND, the CL pin must be connected to the device GND.

What about the other pins that require a GND connection?

For example pin IN: in my design is an external pull-down resistor that acts as working resistance of an optocoupler output. To which GND should it be connected?

other pins: DIAG_EN, DELAY.

Regards, Oliver.