This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLVM13610: Schematic review

Part Number: TLVM13610

Tool/software:

Hello,

I request a review of my schematic with TLVM13610. I would like to send the schematic via private message, if possible.
This is a device that takes 15V 3A in using USB Power Delivery, Converts it to 5V using the TVLM13610, and has an output of up to 7A at 5V DC. The output should support a wide range of loads, as this will be used as a 5V power supply.

In short, this device is intended to:
- Convert the input voltage of 15V to 5V
- Require the input voltage to be more than 13V before enabling 5V output
- Meet CISPR 32 Class B emissions


I appreciate your support and am looking forward to your reply.

Best regards,
Mikael