This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25985: DVDT pin question

Part Number: TPS25985

Tool/software:

Hi team,

My customer has some questions on TPS25985 DVDT pin.

1. From recommend operating condition, it shows 4V as min, how to understand the explanation on this? adding the ABS condition, does that mean to this pin should work at 4V~5.5V?

2. When customer is having some experiments, voltage on DVDT is 0.8V, this causes some confusion. So far only one condition to verify as a good design is based on Fig 9-5 in DS. But the cap is 33nF, customer is using 100nF.

3. Does voltage on DVDT pin vary due to cap value? What's the normal operating voltage? Is that 0.8V?