This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5045: LM5045MH/NOPB peak gate current

Part Number: LM5045
Other Parts Discussed in Thread: LM5116,

Tool/software:

Hello,

I am on the way to optimize the EMI behaviour of our buck converter circuit with the LM5116MH/NOPB controller. The Vin is something between 58V...80V and Vout=48V for Pout: 0W...550W. Unfortunately, there is a problem with the external gate resistors we are using for the 1x low side and 2x high side MOSFETs. 

According to the LM5116 datasheet (page 9 & 10) we are allowed  to use the driver source current of  appr. 3.2A for LO and 1.8A for HO and the driver sink current fo 2.9A for HO and 6.8A for LO at the Vcc=12V. 

There is a need to switch off very fast and to switch on a little bit slower to avoid high ringing amplitudes during the switching process. We want to avoid the use of different external gate resistors like the typical application is showing that on page 21 in the datasheet but doesn't that mean, that you will always overdrive the LM5116 internal gate driver with the peak gate currents of Q1 & Q2 (Si7850) ?

Maybe there is an explanation for driving external switch MOSFETs without adding the gate resistors that I do not know?

 

Best regards

 

Dirk.