Other Parts Discussed in Thread: PMP9256
Tool/software:
please share the schematic and BoM of evaluation board with transformer PA2398NL.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Sangramsinh,
Thanks for using the e2e forum.
If you are referring to one of our EVM boards, please have a look at the according User's Guide, which can be found in the technical documentation section.
This file includes a BOM list.
If you are looking for the datasheet of a component listed, you can simply browse the component name at the manufacturer website and download the datasheet from there.
Best regards,
Niklas
Hi Niklas,
I am using PMP9256 EVM board. But i found some mismatches in component values with BoM and schematic also there is no footprint/ placement provision for few components.
could you provide exact BoM for EVM using transformer with part no. of PA2398NL.
Also in BoM inductance for above transformer is 307uH but in actual datasheet of transformer they mention 100uH. please confirm the same.
Hi Sangramsinh,
Thanks for pointing this out.
I will check the schematic and BOM mismatch and see if a revision is necessary.
Please allow me time until tomorrow to get back to you.
Best regards,
Niklas
Hi Sangramsinh,
I agree the schematic is rather confusing here.
In fact, the PCB uses two different inductors X1_A and X2_B.
Only one is populated and only the X1_A is listed in the BOM document.
I assume they created footprints for both inductors to compare the performance of each of them.
Unfortunately, I cannot see which of the two inductors was considered the better selection, but depending on your design requirements, you can also choose which of the two inductors would be more suitable for your design, or even choose a completely different part.
I also recommend to check our power stage designer tool to assess which inductance leads to which current levels within the system.
https://www.ti.com/tool/POWERSTAGE-DESIGNER
Best regards,
Niklas
The BOM can be found here.
https://www.ti.com/lit/df/snvr389a/snvr389a.pdf
Best regards,
Niklas
Hi Sangram,
If the inductance varies between the BOM and the datasheet, I would always follow the datasheet of the components.
In this case, I would calculate with 100uH inductance.
The datasheet gives also information about the footprint necessary for the component to fit.
Please make sure that the winding are connected correctly, otherwise primary and secondary side will conduct current at the same time and you will not get the required power to the output side.
Best regards,
Niklas