Tool/software:
Hello,
I'm using the TPS53681 but I'm only using channel A and not channel B. What do I do with the pins of channel B?
Right now I have them hooked up in this way:
BVSP and BVSN: no connect
BPWM1 and BPWM2: no connect
BCSP1: ground
BCSP2: V3P3
BTSEN: no connect
BVR_RDY: pulled to 3.3V with 10k resistor
BVR_EN: pulled to ground with 10k resistor
Is this correct?
Thanks,
Ryan