This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5168-Q1: 48V DCDC recommendation

Part Number: LM5168-Q1

Tool/software:

Hi expert,

My customer is looking for a suitable DCDC/ LDO to meet below request, do you think LM5168-Q1 is most suitable device for customer or do we have cheaper device than LM5168-Q1?

  • VIN: 48V (MAX VIN > 70V)
  • VOUT: 5V
  • IOUT: 30mA

Best Regrads,

Ryker