Other Parts Discussed in Thread: TPS25751, , BQ25798
Tool/software:
Hi,
I am using the BQ25792RQMR IC for battery charging and the TPS25751 as the PD controller in my project. We have dual power inputs:
-
USB Type-C (VAC1), which is detected and controlled by the battery charger.
-
Pogo pin connection (VAC2), which provides a secondary power source.
Among these, only the Type-C input supports fast charging. We are using a 4S battery configuration, with the charging voltage set to 16.8V and charging current configured to 3A via register settings.
Questions:
-
Behavior with Limited Input on VAC2:
If the supply is switched to VAC2 (Pogo Pins), where the maximum input available is 5V at 2A, will the battery charger automatically adjust the charging voltage and current?-
Does the input voltage dip in an attempt to maintain the default 16.8V/3A charging setting?
-
Or is there an internal mechanism in the BQ25792 that dynamically adjusts the charge parameters based on the available input power?
-
-
Configuration Adjustment for VAC2 Detection:
-
How can I modify the charging current and voltage settings dynamically when VAC2 is detected to avoid potential power dips?
-
Does the BQ25792 provide a built-in configuration method to handle different input sources efficiently?
-
Additionally, could you recommend a suitable fuel gauge IC for a 4S battery configuration?
Thanks in advance!