This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92633-Q1: Schematic Review

Part Number: TPS92633-Q1
Other Parts Discussed in Thread: TPS92633

Tool/software:

HI Team,

Hope all is well.

My customer is Xingyu.

Currently they want to use this device for platform design, so they hope to have a standard schematic design that can be used in different projects.

I understand that the input and output conditions are uncertain and a complete review cannot be conducted. Can you review the parts that can be conducted, and help me point out the parts that need to be determined? I told the customer that this needs to be determined. 

TPS92633.pdf

BR

Link

  • Hi Link,

    Please provide the following:

    1. Input supply voltage operating range
    2. Desired output current for each channel
    3. Min/Max total LED load forward voltage for each channel
    4. Desired FAULT pin function (one-fails-all-fail, Output to MCU for monitoring, etc.)

    Regards,

    Zach