This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR60420: XLMR604205SRAKRQ1

Part Number: LMR60420

Tool/software:

I want below information for XLMR604205SRAKRQ1 MPN on urgent basis

DESCRIPTION MATCHES WITH MPN (YES/NO)?
CORRECT ORDERABLE PART NUMBER
IS THIS PART AVAILABLE IN T&R PACKAGING (YES/NO).?
IF YES, PROVIDE CORRECT ORDERABLE TAPE AND REEL PART NUMBER
STATUS (ACTIVE OR OBSOLETE OR NRND) 
IF NRND, PLEASE PROVIDE LTB AND LTS DATE 
IF OBSOLETE, SUGGEST EXACT DROP-IN REPLACEMENT
PACKING (TAPE & REEL, ROLL, TRAY, TUBE AND BULK) 
PACKAGE/CASE SIZE ( in inches)
MOISTURE SENSITIVITY LEVEL (MSL)
PART-MARKING/TOP MARKING
MOUNTING TYPE: (SURFACE MOUNTED/THROUGH HOLE)
ROHS COMPLIANT WITHOUT ANY EXEMPTION (YES/NO)
IS THIS PART AEC QUALIFIED (YES/NO)
IF AEC QUALIFIED THEN IS IT PPAP CAPABLE ? (YES/NO)
IF ITS NOT AEC AND PPAP CAPABLE, PLEASE SUGGEST EXACT REPLACEMENT WITH SAME FORM, FIT & FUNCTION
DATASHEET LINK