Tool/software:
Hello,
We intend to use the component in IBB configuration and I have a few questions:
- It is stated in the datasheet that the feedback resistors sum must be below 100kOhm. However, in the IBB pspice simulation, the resistors sum is way higher than that.
Does it mean there are specificities in that configuration ? Our goal is to generate a -15V from a 15V, so I was targeting a 49.9k and a 3.57k. - In the application note, you state that a schottky diode should be put, do you have any suggested part or constraint for part selection ?
Best regards,
Clément